Press Release

<< Back
Jun 08, 2020
FLIR Systems Launches FLIR Screen-EST Software to Improve Skin Temperature Screening for COVID-19

FLIR Screen-EST is Available for Use with FLIR Thermal Imaging Cameras Used for Skin Temperature Screening, Offering a Faster Solution for High Traffic Areas

ARLINGTON, Va.--(BUSINESS WIRE)--Jun. 8, 2020-- FLIR Systems, Inc. (NASDAQ: FLIR) today announced the FLIR Screen-ESTTM software for FLIR T-Series, Exx-Series, and A-Series thermal imaging cameras. The software provides automatic measurement tools that perform elevated skin temperature screenings of individuals in two seconds or less at entries, checkpoints, and other high-traffic areas while maintaining recommended social distancing guidelines.

This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20200608005131/en/

New FLIR Screen-EST software designed for use with FLIR thermal imaging cameras used for skin temperature screening offers faster solution for high traffic areas. (Photo: Business Wire)

New FLIR Screen-EST software designed for use with FLIR thermal imaging cameras used for skin temperature screening offers faster solution for high traffic areas. (Photo: Business Wire)

“Governments and businesses across the globe are hard at work developing new processes to ensure public health and safety from COVID-19, including the use of radiometric thermal imaging cameras as part of a comprehensive frontline screening program,” said Jim Cannon, President and CEO at FLIR. “Now with FLIR Screen-EST software, those organizations can increase the speed and accuracy of frontline screening when using FLIR’s thermal cameras.”

The FLIR Screen-EST Method

FLIR Screen-EST software is designed to automatically take a skin temperature measurement near the tear duct of each person, the surface area most closely correlated to core body temperature. When used with T-Series, Exx-Series, or A-Series cameras, the software enables screening of individuals to occur 50 percent faster than FLIR Systems’ existing on-camera screening mode, accelerating throughput. If the software detects a skin temperature that exceeds a threshold set above the baseline average, Screen-EST will notify the operator and display or sound an audible alarm on the subject’s viewing monitor. The individual then should be directed to a secondary medical screening*.

Honed through nearly two decades of experience designing and manufacturing thermal measurement solutions for skin temperature screening, Screen-EST automatically takes skin temperature samples at the screening location to determine an average skin temperature baseline. It then adds additional samples throughout the day. This relative temperature screening method helps accounts for regular body temperature fluctuations caused by natural biological and external environmental factors, thus reducing the amount of inaccurate readings that can impact absolute temperature alarm systems.

FLIR Screen-EST software is for Windows-based laptops and desktops. It offers a plug-and-play connection for FLIR thermal imaging cameras and can be installed or removed within minutes. This provides additional flexibility for operators to easily move locations or to quickly detach the camera for other purposes, including facilities maintenance or machine inspection.

FLIR Screen-EST software for T-Series cameras is available for purchase globally today for $595 USD, 595€ EUR, and 499£ GBP in English only on FLIR.com and through FLIR authorized distributors. Screen-EST software for Exx-Series and A-Series will be available in later this month. To learn more, please visit www.flir.com/screen-est.

* FLIR cameras are for frontline skin temperature screening only. They do not detect fevers, viruses or any specific medical ailment. Anyone who exhibits an elevated skin temperature must receive secondary screenings conducting by medical personnel with medical-grade equipment to determine a diagnosis.

About FLIR Systems, Inc.

Founded in 1978, FLIR Systems is a world-leading industrial technology company focused on intelligent sensing solutions for defense, industrial and commercial applications. FLIR Systems’ vision is to be “The World’s Sixth Sense,” creating technologies to help professionals make more informed decisions that save lives and livelihoods. For more information, please visit www.flir.com and follow @flir.

Media Contact:
Eleana Stayer
FLIR Systems
Phone: +44 7545 204375
Email: eleana.stayer@flir.com

Investor Relations:
Lasse Glassen
Addo Investor Relations
Phone: 424-238-6249
Email: lglassen@addoir.com

Source: FLIR Systems, Inc.