Press Release

<< Back
Jan 07, 2019
FLIR Launches Second Generation Thermal Camera for Self-Driving Cars and New Thermal Handheld for Automotive Repair

Company Unveils Self-Driving Test Vehicle Featuring Automatic Emergency Breaking Enabled by Thermal Cameras

WILSONVILLE, Ore.--(BUSINESS WIRE)--Jan. 7, 2019-- FLIR Systems, Inc. (NASDAQ: FLIR) today announced two thermal imaging cameras for the automotive industry, its next-generation thermal vision Automotive Development Kit (ADK™) for the development of self-driving cars and a handheld diagnostic thermal camera for auto enthusiasts and professionals, the FLIR TG275.

This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20190107005342/en/

FLIR’s second generation all-weather thermal-vision automotive development kit (ADK) augments other  ...

FLIR’s second generation all-weather thermal-vision automotive development kit (ADK) augments other autonomous vehicle sensors and offers the redundancy needed to improve safety. (Photo: Business Wire)

FLIR also unveiled a thermal enhanced self-driving test vehicle that demonstrates how thermal cameras improve the safety of advanced driver-assistance systems (ADAS) and fill performance gaps in the autonomous vehicles (AV) of tomorrow. The new cameras and the FLIR thermal autonomous test vehicle will be demonstrated this week at the 2019 Consumer Electronics Show (CES) at the Las Vegas Convention Center, South Hall Three, booth #31166.

Next-Generation FLIR ADK

The next-generation thermal-vision ADK featuring the high-resolution FLIR Boson® thermal camera core is designed to help automakers, tier-one automotive suppliers, and automotive innovators improve the safety of ADAS and self-driving vehicles. Paired with machine-learning algorithms for object classification, the ADK provides critical data from the far infrared portion of the electromagnetic spectrum to improve the decision making of AVs in common environments where other sensors experience challenges, such as darkness, shadows, sun glare, fog, smoke, or haze. The thermal-vision ADK augments the entire sensor suite and offers the redundancy needed to improve safety in AVs.

The new ADK is IP67 rated and now includes an integrated heated window for improved performance in all-weather testing. It also features Gigabit Multimedia Serial Link (GMSL), USB, and Ethernet connection for easier integration. The FLIR ADK is available for purchase at www.flir.com/adk.

FLIR’s Autonomous Test Vehicle

FLIR is also showing the industry’s first thermal camera-equipped commercial test vehicle featuring multiple FLIR ADK cameras that will provide a 360-degree street view. The car demonstrates the ADK’s integration capabilities with radar, LIDAR, and visible cameras found on autonomous test vehicles today. With thermal camera-enhanced automatic emergency braking (AEB), the car helps validate how thermal imaging with machine learning classification improves the functionality of AEB.

“For automated decision making on the roadway, thermal imaging cameras coupled with machine-learning capabilities provide the most effective method for pedestrian detection to save lives, particularly in cluttered environments or in poor visibility,” said Jim Cannon, President and CEO at FLIR. “Furthermore, the FLIR thermal-enhanced autonomous test vehicle demonstrates how thermal cameras can significantly improve urban, highway, and AEB performance and the overall safety of self-driving cars.”

Autonomous car developers interested in more information on the thermal-enhanced test vehicle may visit www.flir.com/adas.

FLIR TG275

The TG275 is FLIR’s first dedicated thermal camera for automotive technicians and home mechanics. In automobile repair, heat can often mean a potential issue, and the TG275 helps technicians spot problems before they lead to failures, and ultimately a roadside breakdown. Equipped with the FLIR Lepton® thermal microcamera, FLIR’s patented MSX® technology extracts high-contrast details from the images taken by an onboard visible light camera and superimposes them onto the thermal images. Also, the TG275 allows auto repair technicians to reduce diagnostic time and show customers evidence of the problem through before and after images of potential issues.

The TG275 will be available this spring. For additional information, visit www.flir.com/tg275.

About FLIR Systems, Inc.

Founded in 1978 and headquartered in Wilsonville, Oregon, FLIR Systems is a world-leading maker of sensor systems that enhance perception and heighten awareness, helping to save lives, improve productivity, and protect the environment. Through its nearly 3,500 employees, FLIR’s vision is to be “The World’s Sixth Sense” by leveraging thermal imaging and adjacent technologies to provide innovative, intelligent solutions for security and surveillance, environmental and condition monitoring, outdoor recreation, machine vision, navigation, and advanced threat detection. For more information, please visit www.flir.com and follow @flir.

Source: FLIR Systems, Inc.

Media Contact
Tim McDowd
503-498-3146
tim.mcdowd@flir.com

Investor Relations
Jay Gentzkow
503-498-3809
jay.gentzkow@flir.com